Product added to cart
Athermal
 

ATHERMAL

RUGGEDIZATION

      •   Designed to Maintain High Resolution Over a Wide Temperature Range
      •   Covers a Wide Range of Sensors Up to 1.1”
      •   Optothermal Stability from Passive Athermalization

All matter expands or contracts in response to temperature change. In a lens, this means that focus will drift with temperature. High-performance vision systems require athermalized imaging lenses which are ruggedized to compensate for this phenomenon. Athermalization can be active or passive and each type has its benefits. Additional information about the types of athermalization can be found in An Introduction to Passive Athermalization.

The TECHSPEC® Athermal Imaging Lenses are athermalized imaging lenses which are the result of a collaboration between Edmund Optics and Ruda-Cardinal, a leader in the field of optical engineering, specializing in the design and development of cutting-edge optical systems. Combined efforts enabled rapid and reliable development of this lens, designed to meet a wide array of applications with affordability, availability, and volume manufacturing in mind.

As the ambient operating temperature changes from -10°C to 50°C, the point of best focus for the non-athermalized lens design, shown in the top figure, also changes. The athermalized lens design shown below is protected from this change in temperature. This animation is not to scale.
As the ambient operating temperature changes from -10°C to 50°C, the point of best focus for the non-athermalized lens design, shown in the top figure, also changes. The athermalized lens design shown below is protected from this change in temperature. This animation is not to scale.

Edmund Optics® Athermal Imaging Lenses

  • Designed to Maintain High Resolution Over a Wide Temperature Range
  • Ruggedized for Shock and Vibration Environments
  • Large Sensor Coverage up to 1.1”
  • Optothermal Stability from Passive Athermalization
  • 2022 Silver VSD Innovators Award Winner and 2022 Inspect Award Nominee

Need a custom, ruggedized solution for a demanding application?

Whether you need a build-to-print custom imaging lens or a custom lens designed to specific functional requirements, our engineers provide ideal solutions catered to the unique and challenging demands of the most nuanced imaging applications. With our comprehensive in-house manufacturing capabilities, Edmund Optics® is committed to providing the best solution at every step of the way.

Learn More  

Want to Learn More About Athermal Ruggedization?

 

Athermalization Ruggedization

Read
 

An Introduction to Passive Athermalization

Read
 

Thermal Properties of Optical Substrates

Read
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin