eo_logo
 
Product added to cart

Minimize Unwanted Stray Light!

 

Some amount of light transmits through conventional dielectric mirrors

 

Unwanted transmitted light introduces noise and makes laser systems less safe

 

The opaque substrate of Schwarz Mirrors absorbs this unwanted light

 

An engineered fused silica substrate maintains key properties of fused silica

Please accept marketing-cookies to watch this video.

To prevent unwanted light transmission in laser systems, beam dumps are often placed behind every dielectric mirror. Though highly-reflective, a small amount of light always leaks through dielectric mirror coatings. This unwanted transmission can pass directly through the mirror substrate or create ghost reflections within it, decreasing laser system performance and even creating laser safety issues.

Edmund Optics' new Schwarz Mirrors can significantly reduce the need for beam dumps behind components. These mirrors are novel optical components that use opaque, engineered fused silica substrates that reduce light propagation through the mirror by several orders of magnitude while maintaining >98% of the mirror's reflective properties. The substrate itself appears black, (the word schwarz being German for black), while the beneficial properties of fused silica are maintained. Using a Schwarz Mirror can minimize the size of optical systems and improving safety by eliminating stray laser light.

What’s Wrong with Conventional Mirrors?

While the majority of incident laser light is reflected by dielectric mirror coatings designed for those wavelengths, some amount of light will always transmit through the coating into the substrate. Fused silica and other common mirror substrates may allow this light to transfer out of the back of the mirror or create a ghost reflection, introducing stray light into the system. Wavelengths outside of the reflection band of the mirror may also pass through the mirror and further contribute to system noise, reducing system performance.

What Makes the Substrates of Schwarz Mirrors Special?

Schwarz Mirrors are constructed from an engineered fused silica that maintains the high laser-induced damage threshold (LIDT) and low thermal expansion of fused silica while also blocking unwanted light transmission (Figure 1). They feature a typical thermal expansion coefficient of 0.55x10-6/K, are opaque, and essentially function as neutral density filters.

Figure 1: The engineered fused silica substrates of Schwarz Mirrors (left) maintain the high LIDT and low thermal expansion coefficient of traditional fused silica (right) with the added benefit of absorbing unwanted light that would otherwise propagate through the mirror substrate and leave the back surface.

Schwarz Mirrors: Blocking Unwanted Transmission

Figure 2 demonstrates the superior light blocking of a Schwarz Mirror's engineered fused silica substrate. This eliminates the need for beam dumps to be placed behind mirrors, which reduces the total system cost, weight, and size.

Figure 2: Laser light leaks out of the back surface of a conventional dielectric mirror with a fused silica substrate (top) while a Schwarz Mirror with the same thickness, diameter, and coating prevents this unwanted light from passing through the mirror (bottom).

Testing Schwarz Mirror Performance

In order to evaluate the performance of Schwarz mirrors, a 25 mm diameter, 5 mm thick blank of black, engineered fused silica was cut and polished on one side. Transmission through the material was measured using a 532 nm diode-pumped solid-state (DPSS) continuous-wave laser with 500 mW output power and a silicon-based photodiode capable of measuring as low as 500 nW with a 10 nW resolution. No signal was detected, implying transmission of 7.

This blank was thinned and polished to 4 mm, 3 mm, and finally 2 mm without any recordable transmission to further understand the material’s ability to attenuate visible light. Using a lock-in amplifier capable of recording OD up to 9, the 2 mm sample still yielded no transmission for the visible range.

Next, the same laser and photodiode were used to compare a Schwarz Mirror and a conventional dielectric mirror with a fused silica substrate. Both mirrors had a diameter of 25 mm, a thickness of 5 mm, and the same highly-reflective dielectric coating designed for 532 nm. The laser was attenuated to 137 mW and directed onto the mirrors at a 45° as shown in Figure 2. The photodiode recorded measurements both in front of and behind the mirrors to determine reflection and transmission. Figures 3 and 4 combine data from two different Schwarz Mirror samples and two conventional fused silica mirror samples, all of which were measured five times each.

Figure 3: There was minimal change to the reflectivity of Schwarz Mirrors compared to conventional dielectric mirrors.
Figure 4: Schwarz Mirrors had significantly higher optical densities than the conventional mirrors.

The reflected intensity was measured at 12.7 mm (near) and 304.8 mm (far) from each optic over a timeframe of five minutes. On average, these Schwarz Mirrors reflected 118.2 mW of the incident light at the extended distance, achieving 98.7% of the reflection performance of the conventional fused silica mirrors (119.6 mW). In most systems, Schwarz Mirrors could replace conventional fused silica mirrors without noticeable change in reflective performance.

The transmission was measured 304.8 mm behind the optics, on-axis with the incident beam. The conventional fused silica samples transmitted >84 µW of light while the Schwarz Mirrors had no measurable transmission with this source, again transmitting below the photodiode’s threshold of 500 nW.

Schwarz Mirrors at Edmund Optics®

TECHSPEC

Schwarz Mirrors

  • >98% Visible Reflectivity with No Residual Transmission
  • Optical Density > 7.0 in Visible Spectrum
  • Engineered Highly-Absorptive Fused Silica Substrate

FAQs

FAQ  Do the engineered fused silica substrates of Schwarz Mirrors make them more expensive than conventional fused silica mirrors?
Yes, Schwarz Mirrors are slightly more expensive than conventional fused silica mirrors, but they eliminate the need for beam dumps to be placed behind each mirror. This significantly reduces overall system cost, weight, and size.
FAQ  Can Edmund Optics® manufacture custom Schwarz mirrors at different sizes and wavelength ranges?

Yes, Schwarz mirrors can be custom manufactured for different sizes and coating options. It is important to keep in mind that the optical density specification will decrease as the substrates get thinner.

Technical Resources

Application Notes

Technical information and application examples including theoretical explanations, equations, graphical illustrations, and much more.

Highly Reflective Coatings
Read  

Common Laser Optics Materials
Read  

Key Parameters of a Laser System
Read  

UV vs. IR Grade Fused Silica
Read  

Optical Glass
Read  

Edge-Blackening
Read  

Videos

Informative corporate or instructional videos ranging from simple tips to application-based demonstrations of product advantages.

Introduction to Laser Optics Lab 
Watch  

Metrology at Edmund Optics: Measuring as a Key Component of Manufacturing 
Watch  

Schwarz Mirrors –
TRENDING IN OPTICS: EPISODE 4 
Watch  

Webinars

Recorded webinars from Edmund Optics® experts on a wide range of optics and imaging topics.

High Reflectivity Mirrors for Laser Applications
Watch  

Was this content useful to you?
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin