eo_logo
 
Product added to cart

Beam Expander

A component commonly used with lasers to increase the beam diameter. One advantage is that expanding a beam will decrease divergence by the expansion factor. The decreased divergence is a major advantage for long distance applications despite the initial increase in beam diameter. For example, a 1mm laser beam expanded 10X will be 10mm in diameter and will have one tenth the divergence of the original beam.

See also Beam Divergence , Beam Diameter

Was this content useful to you?
 
Sales & Expert Advice
1-800-363-1992
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin