eo_logo
 
Product added to cart
Transcelestial

Case Study:
How Transcelestial and
Edmund Optics are Bringing the Internet to Everyone, Everywhere

The future depends on global access to affordable, lightning-fast wireless communication

Re-imagining Wireless Communications
for a Connected World

Wireless laser communication can bring internet access to anyone anywhere in the world. Transcelestial, a start-up company based in Singapore, is working on a prototype that will wirelessly transmit data at faster speeds, greater distances, and a lower cost than current wireless technology by utilizing free-space optical communication. Transcelestial is looking to utilize a network of nanosatellites to transfer data using ultra-thin laser beams to telescope-like ground stations. Just as ground-based communications have evolved from using copper wiring to fiber optics in order to improve speed and efficiency, Transcelestial is aspiring to create the next evolution of wireless communications. The current standard for wireless communication is to transmit information over radio frequencies but light waves are able to transmit data much faster. Fiber optics are also expensive to install and replace because of labor and digging costs.

Transcelestial found that standard components from Edmund Optics® (EO) could help them quickly prototype and create multiple design iterations to find an optical solution that worked for their needs. The dedicated engineering support they received from Edmund Optics’ startUP program helped them narrow in on their options and identify the exact components needed for the project. Edmund Optics quickly replied to sales requests, assisted the company with discounts, and offered flexible payment options that allowed Transcelestial to get the necessary products to work on their prototype first without having to pay for them right away.  

As of 2017, only 48% of households worldwide have access to the internet.1

Improving Global Education, Employment, and Health

The internet has become essential to success in the modern world and ubiquitous wireless laser communications can make it more accessible and efficient. Providing affordable internet access worldwide will drastically improve the living conditions of those in emerging countries and low-income families.

Having access to the internet benefits one’s education, employment, health, and other various aspects of life. The abundance of available online resources can teach valuable life skills and even let people earn online college degrees that would have been otherwise unobtainable. Internet access also provides many more options for employment, allowing people to search through a wealth of available jobs and create online businesses with access to far more customers than they would otherwise be able to reach. Internet access also improves the health of communities by educating them about medical conditions and allowing them to seek help when necessary. Figure 1 shows the proportion of households with access to the internet across different communities worldwide.  

57.1% of households in developing countries and 85.3% of households in “least developed countries”
Figure 1: 57.1% of households in developing countries and 85.3% of households in “least developed countries” (LDCs) do not have internet access1 * Estimates. CIS refers to the Commonwealth of Independent States and LDC refers to least developed countries

Reducing the Number of Aircraft Disappearances

In addition to helping low-income communities and developing countries, global wireless internet access can also improve the connection between ground control and aircrafts, reducing the amount of aircraft disappearances. Aircraft traveling over the ocean make periodic checks with air traffic controllers over the radio, but have no high-speed connection to send real-time data to ground control. Being able to communicate throughout an entire flight will allow ground control to monitor and correct any issues both effectively and quickly. Transcelestial’s satellite network solution for providing a high-speed internet connection that is globally accessible at all times would prevent airplane disappearances, like the Malaysia Airlines Flight MH370, from happening again (Figure 2).  

83 aircraft have disappeared without a trace between 1948 and 2014 and the majority of missing flights were passenger planes
Figure 2: 83 aircraft have disappeared without a trace between 1948 and 2014 and the majority of missing flights were passenger planes2

What is Wrong with Current Wireless Technology?

With the expansion of the internet comes a demand for higher bandwidth in order to compensate for the increase in data. There is an almost 10X growth in data expected in the next 5 years. However, the current dependence on radio frequencies for wireless communication has several drawbacks. Radio waves have long wavelengths that require cumbersome hardware, such as massive underground cables or large dish antennae, to transmit and receive information. This equipment is expensive and hard to implement in remote places. Laser beams have much more bandwidth than radio frequencies, which allows them to carry more data at a fraction of the cost.

Challenge

The needs of a startup company like Transcelestial are very different from those of a larger company. Startups are typically racing to meet product deadlines, secure investors, and beat their competition to market. This makes them more time-sensitive than larger, more established companies and heavily dependent on rapid prototyping. Startups are also more cost-sensitive than larger companies are and must find creative ways to develop their products while minimizing expenses. Transcelestial needed to be able to quickly prototype different optical solutions and continuously iterate until they found a design that worked for their demanding needs.

Solution

Edmund Optics was able to help Transcelestial rapidly develop the prototypes the company needed by providing dedicated engineering support and shipping critical stock components out same day. These products included prisms, filters, lenses, mirrors, optical tables, and optomechanics. Edmund Optics answered any questions that arose and gave Transcelestial advice on which optical components would work best in the system. This resulted in an optical prototype that met all of Transcelestial’s demanding requirements. Edmund Optics also provided Transcelestial with flexible payment options that allowed them to experiment with different components for the prototype without having to pay right away. Rohit Jha, the CEO and co-founder of Transcelestial, stated that Edmund Optics provided "rapid sales response on requests for orders, even if some of them are very urgent and quite last minute for the day."

Transcelestial is a member of Edmund Optics’ startUP program, which seeks to create an environment where new and expanding businesses can focus on what matters most, continuing to innovate and grow their business. The startUP program offers member discounts, dedicated engineering support, and personalized solutions.  

"Edmund Optics has been our choice local optics supplier since Day 1."
- Rohit Jha; CEO & Co-Founder
Transcelectial Quote
Was this content useful to you?

References

1 Sanou, Brahima. “ICT Facts and Figures 2017” International Telecommunications Union, July 2017.

2 “Statistics.” Aviation Safety Network Flight Safety Foundation, Jan. 2018, aviation-safety.net/statistics/.

The Future Depends on Optics
 
Sales & Expert Advice
 
or view regional numbers
Easy-to-Use
QUOTE TOOL
enter stock numbers to begin