Edmund Optics® (EO), the premier provider of optical components, introduces new Linear Variable Bandpass Filters. These versatile filters provide the high transmission and deep rejection necessary to isolate narrow spectral regions for use in a wide variety of applications.
Narrow bandwidths with high transmission
Linear Variable Bandpass Filters are precision coated optical filters featuring spectral properties that vary linearly across the length of the filter. They provide an optimum input beam diameter of 0.5 x 10.0mm. Delivering OD4 blocking, these filters provide high transmission across narrow bandwidths. They offer impressive blocking of greater than 4.0 optical density at just 1.5% of the laser wavelength. Deep blocking of unwanted light maximizes system performance at the required wavelength. The spectral response can be conveniently adjusted by simply moving the filter’s position relative to the light source. A single Linear Variable Bandpass Filter can replace multiple dedicated filters, which simplifies system setup and minimizes weight for optimal value.
Available in VIS and NIR models
Linear Variable Bandpass Filters are available in VIS and NIR models. They are in-stock and available for immediate delivery for fast turnaround and excellent value.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics India Private Limited, #267, Greystone Building, Second Floor, 6th Cross Rd, Binnamangala, Stage 1, Indiranagar, Bengaluru, Karnataka, India 560038
California Consumer Privacy Acts (CCPA): Do Not Sell or Share My Personal Information
California Transparency in Supply Chains Act
The FUTURE Depends On Optics®