Edmund Optics® (EO), the premier provider of optical components, announces the new TECHSPEC® Compact Ruggedized (Cr) Series Fixed Focal Length Lenses. These Stability Ruggedized versions of our popular TECHSPEC® C Series Fixed Focal Length Lenses are designed to maintain optical pointing and positioning in harsh environments that involve vibration, shock, and changing temperatures. The individual lens elements are glued in place inside the barrel to prevent lens element decenter during shock and vibration. Pixel shift is reduced, thereby eliminating object shift on the image and ensuring that the object to image mapping remains constant. A point on the object will always map to the same point on the image even after the lens has been heavily vibrated or shocked.
TECHSPEC® Cr Series Fixed Focal Length Lenses offer a simplified focus with a wide range of aperture options. Available in four focal lengths from 6mm to 25mm, these Stability Ruggedized C-mount lenses feature robust mechanics and a stainless steel locking C-mount clamp. TECHSPEC® Cr Series lenses are ideal for calibrated imaging systems such as measurement, gauging, 3D stereo vision, robotics, sensing, and autonomous vehicles.
“Today, more and more applications require Stability Ruggedization. This is driven not only by demands for higher levels of measurement accuracy, but also by recent changes in sensor technology – pixels are reducing drastically in size to approach 1 micron – which significantly reduces the tolerance for misalignment of the system optics,” says Greg Hollows, Imaging Business Unit Director at Edmund Optics. “The Cr Series of ruggedized lenses maintain their optical performance in these challenging conditions while delivering the exceptional quality that the industry has come to expect from every Edmund Optics lens.”
TECHSPEC® Cr Series Fixed Focal Length Lenses are in-stock and available for immediate delivery for fast turnaround and excellent value. For more information, click here.
About Edmund Optics:
Edmund Optics® is a leading supplier of optics, imaging, and photonics technology for the Life Sciences, Biomedical, Semiconductor, R&D, and Defense markets around the globe. Edmund Optics designs and manufactures a wide array of multi-element lenses, lens coatings, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of both stock and custom products. Edmund Optics’ state-of-the-art manufacturing capabilities, combined with its global distribution network, has earned it the position of the world’s largest supplier of off-the-shelf optical components. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics India Private Limited, #267, Greystone Building, Second Floor, 6th Cross Rd, Binnamangala, Stage 1, Indiranagar, Bengaluru, Karnataka, India 560038
California Consumer Privacy Acts (CCPA): Do Not Sell or Share My Personal Information
California Transparency in Supply Chains Act
The FUTURE Depends On Optics®