Edmund Optics® (EO), the premier provider of optical components, continuously expands its product offering to reflect market developments and customer needs. New products are added each month to better serve the industry. This release features details about the recent additions including Colored Glass Diffusers and TECHSPEC® Low GDD Ultrafast Mirrors.
The new Edmund Optics Colored Glass Diffusers feature SCHOTT color glass filter substrates that are 120-grit sandblasted on one side to create a diffuse, light scattering surface. These diffusers exhibit the same transmission and blocking bands as their colored glass filter substrates. Colored glass diffusers are ideal for applications where a single white light source is being used to create diffuse, colored illumination at different wavelengths, rather than using multiple LEDs.
Edmund Optics TECHSPEC® Low GDD Ultrafast Mirrors are designed to have high reflectivity at a 45° angle of incidence for ultrafast laser beam steering applications. The low group delay dispersion (GDD), high-reflectivity coating, obtained through a precision ion beam sputtering (IBS) process reduces scatter and absorption better than traditional dielectric laser mirrors. TECHSPEC® Low GDD Ultrafast Mirrors feature near-zero GDD at their design wavelength range, minimizing dispersion of the reflected beam and making them ideal for the transport of femtosecond laser pulses.
To view these products and the many more exciting new products offered at Edmund Optics®, visit the new products page at edmundoptics.com.
About Edmund Optics:
Edmund Optics® (EO) is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. Edmund Optics designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. With locations in more than seven countries across the globe, Edmund Optics employs over 1,000 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics India Private Limited, #267, Greystone Building, Second Floor, 6th Cross Rd, Binnamangala, Stage 1, Indiranagar, Bengaluru, Karnataka, India 560038
California Consumer Privacy Acts (CCPA): Do Not Sell or Share My Personal Information
California Transparency in Supply Chains Act
The FUTURE Depends On Optics®